ufSession.Ugmgr.DecodePartFileName() returns an MFK string.
The above function is affected by MFK setting.If the Teamcenter preference TC_NX_Supports_MFK is set to True,the behavior of the function will be as below according to the document.
In case of Default Domain: it is Teamcenter Engineering item ID. In case of non-Default Domain: it is the multifield key. e.g. ,=item_id=001, object_type=Document ,=item_id=001, object_type=SupplierPart, supplier_code=x
The default domain is set by the Teamcenter PreferenceTC_MFK_DEFAULT_DOMAINThe default value is Item:
TC_MFK_DEFAULT_DOMAIN=Item